Technical FAQs

Ask a Question

RTC Synchronization with Time Zone over Internet in M172 performance controller

M17xP supports this BIBBS (Bacnet interoperability building blocks): 
DM-TS-B(*) TimeSynchronization-B 
so a Bacnet supervisor can synchronize it. 

NTP (Network time protocol) is most common and widely used network protocol among the protocols used for clock synchronization of device over network 
Today NTP / SNTP is not supported on M17xP controllers so it is not possible to synchronize the RTC of it to the NTP server.

 
Was this helpful?
What can we do to improve the information ?