Technical FAQs

Ask a Question

What is the part reference for M580 Hot Standby copper link.

If we use a 490NAC0100 copper transceiver, you can elect to use either of the following 5m ethernet shielded twisted pair Cat5e straight copper cables to make the Hot Standby connection:

1. 490NTW00005 : CE-compliant
2. 490NTW00005U: UL-compliant.
 
Was this helpful?
What can we do to improve the information ?