Technical FAQs

Ask a Question

Is it possible to replace TM258LF42DTS0 by TM258LF42DT.

TM258LF42DTS0 is the Solution Extension module.
In the past, there was two software; one is SoMachine and second one is SoMachine solution extension.
On ‘So” controller , it  was programmed by SoMachine solution extension .In this case , there was a solution library .So, for example, on this TM258LF42DT ,in past, we cannot use solution library.
However; it is possible to replace TM258LF42DTS0 by TM258LF42DT but need to update the firmware V4.0.3.2.
For your information; SoMachine 4.3 have already integrated all the solution library. you need to upgrade the Firm ware of TM258LF42DT by V4.0.3.2
Was this helpful?
What can we do to improve the information ?