Technical FAQs

Ask a Question

How to protect unused slots of modicon X80 Backplane.

If a rack has unused module slots, install a BMXXEM010 cover to keep dust and other objects out of the slots and to comply with IP20 ingress protection requirements.
BMXXEM010 covers are sold in sets of 5. 
Was this helpful?
What can we do to improve the information ?