Technical FAQs

Ask a Question

Is it possible to use controller inside card VW3A3501 with ATV930 drives.

It is not possible to use controller inside card VW3A3501 with ATV930 drives. VW3A3501 is compatible with ATV61 & ATV71 drives only.
You can use M241 and M251 plc or you can select another PLC as per the requirement.
Was this helpful?
What can we do to improve the information ?