Technical FAQs

Ask a Question

How to select ICD file of ION8650

Onb# correspond with the on board IO available 
1 correspond with A
2 correpond with B 
Please refers to the technical datasheet Pg6
Ext# correspond with the IO expander option 
1 correpond with A 
2 correpond with B
3 correpond with C 
4 correpond with D
Please refer to the technical datasheet Pg7, 
here is a link:  http://www2.schneider-electric.com/documents/product-services/en/product-launch/powerlogic/ION8650_datasheet.pdf

1. Identify the feature set A,B or C 
B for M8650B4C0H6C7A0A - ION8650B 
C for M8650C4C0H6C7A0A - ION8650C 

2. Identify the on board I/O 
A for M8650B4C0H6C7A0A - Onb1 
A for M8650C4C0H6C7A0A - Onb1 

3. Identify the IO expander option, if necessary. 
As an example if the IO expander part number is P850EA2, then A for P850EA2 equals Ext1 
If there is no IO expander then select an ICD without Ext.  

With the example above  
For M8650B4C0H6C7A0A load this ICD file SE_ION_8650-B-Onb1-Exp1-F01_E1V01 
For M8650C4C0H6C7A0A load this ICD file SE_ION_8650-C-Onb1-Exp1-F01_E1V01 
But again this is an example only and the ICD file might differ depending there is an IO Expander 

 
Was this helpful?
What can we do to improve the information ?