Technical FAQs

Ask a Question

what is current consumption for MiCOM P54X IRIG-B un modulated port (input signal level TTL)

External clock synchronization to IRIG standard 200-98, format B00X
Input signal level TTL
Input impedance at dc 10KOhm

current consumption for MiCOM P54X IRIG-B un modulated port is 0.5mA
Was this helpful?
What can we do to improve the information ?