Technical FAQs

Ask a Question

What is the maximum number of records can be stored in PM2000

 Up to two fixed parameters (e.g., kWh and kVAh) with configurable interval and duration  (e.g., 2 parameters for 60 days at 15 minutes interval) Maximum 5760 records.

Was this helpful?
What can we do to improve the information ?