Technical FAQs

Ask a Question

What is the degree of protection for TeSys GV4 motor circuit breakers.

The degree of protection (front face) for TeSys GV4 motor circuit breakers conforms to IEC 60529
-> Open mounted IP 40 front face except on connection area.
-> Connection area:
  • IP20 with EverLink connector
  • IP40 with crimp lug connector and terminal shield.
-> In enclosure DRH (direct rotary handle) = IP40
                         ERH (extended rotary handle) = IP54 or IP65
Was this helpful?
What can we do to improve the information ?