Technical FAQs

Ask a Question

What is the shock resistance of TeSys GV4 motor circuit breakers.

The shock resistance of TeSys GV4 motor circuit breakers conforming to IEC 60068-2-27 is 15g,11 ms.
Was this helpful?
What can we do to improve the information ?