Technical FAQs

Ask a Question

What is the vibration resistance of TeSys GV4 motor circuit breakers.

The vibration resistance of TeSys GV4 motor circuit breakers conforming to IEC 60068-2-6 is
  • 2.0 to 13.2 Hz and amplitude ±1 mm
  • 13.2 to 100 Hz acceleration 0.7 g
Was this helpful?
What can we do to improve the information ?