Technical FAQs

Ask a Question

What is the flame resistance of TeSys GV4 motor circuit breakers.

The flame resistance of TeSys GV4 motor circuit breakers conforming to  IEC 60695-2-11 is 960°C.
Was this helpful?
What can we do to improve the information ?