Technical FAQs

Ask a Question

What is the Maximum conventional rated thermal current (Ith) of TeSys GV4 motor circuit breakers.

The Maximum conventional rated thermal current (Ith) of TeSys GV4 motor circuit breakers Conforming to IEC 60947-4-1 is 115A.
Was this helpful?
What can we do to improve the information ?