Technical FAQs

Ask a Question

Are TeSys GV4P motor circuit breakers suitable for isolation.

Yes, the TeSys GV4P motor circuit breakers are suitable for isolation Conforming to IEC 60947-1 § 7-1-6.
Was this helpful?
What can we do to improve the information ?