Technical FAQs

Ask a Question

What is the use of favourite page in PM1130H meter ?

The PM1130H meter allows you to select 3 parameters and arrange them in required order to
be displayed in favourite page. These parameters can be selected only through
communication and are based customer requirements. Some parameter logs are
of utmost importance and navigating to those parameters takes time. For ease of
navigation and accessibility, the meter allows you to chose 3 parameters and lock
the page for easy reading. The selectable parameters are:
• V L-L
• V L-N
• A
• F
• W
• PF
Was this helpful?
What can we do to improve the information ?