Technical FAQs

Ask a Question

What is the degree of protection of iCMA & iCMV.

The degree if protection of iCMA & iCMV is shown below:

Degree of protection:
– IP66 on front face.
– IP20 at terminal level.
Was this helpful?
What can we do to improve the information ?