Technical FAQs

Ask a Question

What is the temperature information on iCMA & iCMV.

The operating and storage temperature on iCMA & iCMV are shown below:
  • Operating temperature: -20 °C to 55 °C.
  •  Storage temperature: -25°C to 80°C.
Was this helpful?
What can we do to improve the information ?