Technical FAQs

Ask a Question

What is the operating temperature range for iEM2000T meter.

The operating temperature range for iEM2000T meter is as follows:

Operating temperature: -25°C to +65°C if < 32 A
                                  -25°C to +55°C if  >32 A

Storage temperature : -40°C at +70°C.
Was this helpful?
What can we do to improve the information ?