Technical FAQs

Ask a Question

How to resolve "Failed to establish connection with server" error in SBO

If facing the issue  "Failed to establish connection with server" while logging in SBO then you have to check whether software administrator is stopped or not by going to following path :

Windows/All Programs/SchneiderElectricStruxureWare/BuildingOperation/SoftwareAdministartion

Click on the start button. It will start the server and you will be able to login.
Was this helpful?
What can we do to improve the information ?