Technical FAQs

Ask a Question

Which input is used in Tesys T for remote reset.

Yes, the device can be remote reset using both Input 5 and the PLC. 

Not all faults can be reset remotely.
Was this helpful?
What can we do to improve the information ?