Technical FAQs

Ask a Question

Which are overload contacts in Tesys T.

the normally open (terminal 97 and 98), and normally closed (terminal 95 and 96) contacts overload contact and these are isolated contacts.
Was this helpful?
What can we do to improve the information ?