Technical FAQs

Ask a Question

What are the maximum no of LTMR devices which we connect in daisy chain.

Total 16 Modbus TCP / EtherNet IP LTMR device can be connected in daisy chain
Was this helpful?
What can we do to improve the information ?