Technical FAQs

Ask a Question

Does XALG range has good resistance to cutting oil?

The XALG range made of polyamide with fiber glass (PA6 MD30 - Akulon K223-HM6) and it is resistant to cutting oil and more generally to mineral oils.

Was this helpful?
What can we do to improve the information ?