Technical FAQs

Ask a Question

Where should we use Interphase barrier with Masterpact NT& NW ACB ?

If the insulation distance between phases is not sufficient (<=14 mm), it is advised to install phase barriers (taking into account the safety clearances).
Mandatory for a Masterpact NT > 500 V.
Was this helpful?
What can we do to improve the information ?