Technical FAQs

Ask a Question

What are the output contact specification in MiCOM P127 relay?

Below are the output contact specifications for MiCOM P127 relays :- 

Contact relay-> Dry contact Ag Ni
Make current -> Max. 30A and carrry for 3s
Current Carry capacity-> 5A continuous
 
Was this helpful?
What can we do to improve the information ?