Technical FAQs

Ask a Question

What is the operating and storage ambient temperature of Link150?

The ambient operating temperature is -25 to +70 °C (-13 to +158 °F) and the ambient storage temperature is -40 to +85 °C (-40 to +185 °F).

Was this helpful?
What can we do to improve the information ?