Browse FAQs

What is the actual voltage measurement range for RM22TR33.

Published date: 20 June 2019

The actual measurement range is between 304…576V.
<U Min. limit = 380 – (20% x 380) = 304V
>U Max. limit = 480 + (20% x 480) = 576V

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.