Technical FAQs

Ask a Question

Which Ethernet Protocol are supported by PM5560

The PM5560 supports Modbus TCP, BACnet/IP, HTTP, SNTP, SNMP, SMTP and FTP 
protocols and can communicate at data speeds up to 100 Mbps through its 
Ethernet communications port
Was this helpful?
What can we do to improve the information ?