Technical FAQs

Ask a Question

Does the ATV212 drive support ethernet protocol?

Issue:
Does the ATV212 drive support ethernet protocol?

Product Line:
Altivar 212

Environment:
All

Cause:
Communications.

Resolution:
No, the ATV212 drive does not have ethernet communications available.  It supports Modbus RTU, Metasys N2, BACnet, and LonWorks protocols.
Was this helpful?
What can we do to improve the information ?