Technical FAQs

Ask a Question

Is the VW3A1111 keypad compatible for use with the ATV320 drives?

Issue:
Is the VW3A1111 keypad compatible for use with the ATV320 drives?

Product Line:
ATV320 

Environment:
All serial numbers

Cause:
Revision to product firmware. 

Resolution:
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmwares required:
ATV320  V2.9IE37
VW3A1111  V2.0IE51
Earlier versions are not compatible. 

VW3A1111 is supported for use with the ATV6x0, ATV9x0 and ATV340 VFD product lines.
The ATV320 is also compatible with keypads VW3A1101, VW3A1006 and VW3A1007.

Note: Early versions of the ATV320 catalog included the VW3A1111 keypad by mistake, but was removed from the Sept 2018 catalog.
Was this helpful?
What can we do to improve the information ?