Technical FAQs

Ask a Question

Which terminal block can be used to wired-up BMXSAI0410 module.

BMXSAI0410 will be wired-up Via 20-way cage clamp, screw clamp, or spring-type removal terminal block BMXFTB2000/2010/2020.
Was this helpful?
What can we do to improve the information ?