Browse FAQs

Preventa XCS Atex - Are the XCSDMC79*EX or XCSDMC59*EX magnetic switches UL & CSA approved

Published date: 06 June 2019

The magnetic switches XCSDMC79*EX or XCSDMC59*EX are Atex certified by the Ineris certified body according to the european Atex directive 2014/34/EU and the relevant EN standards. They are not UL or CSA certified because the rules are not harmonized in North America. Attached Atex essential guide extract showing the certification of these switches.

Was this helpful?

What can we do to improve the information ?