Technical FAQs

Ask a Question

Video:How to set beeper volume level of SRC6KUXI through the display.

Kindly follow the below steps  to set beeper volume level of SRC6KUXI through the display:

1.Press enter key for the main menu.
2.Select user interface option from the configuration menu.
3.Press enter key beeper volume level will start flashing.
4.Use the navigation key to select the desired beeper volume level and press enter to apply the changes.


 
Was this helpful?
What can we do to improve the information ?