Technical FAQs

Ask a Question

Video:How to run a self test through PCPE.

Kindly follow the below steps to run a self-test through PCPE.

1.Open PCPE application.
2.Select Run Self-Test option under Monitor system. 
3.Click on Run self-test option.
4.Now the self-test is in progress.
5.If there is an issue with input supply, battery or PCB board then the self-test will fail else the self-test will be passed.


 
Was this helpful?
What can we do to improve the information ?