Technical FAQs

Ask a Question

Is there EMC filter in ATV310 drive?

​The ATV310 product is designed as compact machinery drive, so there is no build-in EMC filter inside ATV310. And there is no additional EMC filter available for ATV310. 

It has no EMC filter inside so it does not fulfill the emission level part. It will have some disturbance to other equipment like controller and sensor. 
Was this helpful?
What can we do to improve the information ?