Technical FAQs

Ask a Question

What is the supply voltage limits for ATS22***Q soft starter.

[Us] rated supply voltage for ATS22***Q soft starter is 230...440 V - 15...10 % 
230...440 V - 15...10 % means => 230 x -15% ...440 x10 % =>means =>195.5 V ….484 V 
So, supply voltage limits are 195~484V. 
Was this helpful?
What can we do to improve the information ?