Technical FAQs

Ask a Question

What is the replacement of XUBH043234.

This reference number XUBH043234 was a receiver part of a thru-beam sensor, the transmitter reference was a XUBH0430.
The cross reference of XUBH043234 is a XUB0APSNL2 and for the transmitter the reference is XUB0AKSNL2T.
Very important things to know on a thru-beam: it is not possible to substitute only one part and keep the other, we need to change all. So, in this case; cross reference of XUBH043234  is XUB0APSNL2+ XUB0AKSNL2T.
 
Was this helpful?
What can we do to improve the information ?