Technical FAQs

Ask a Question

Is there any replacement for ACW21M169012.

For this reference ACW21M**9012, There are 2 cable entries: 
- M11 => corresponds to ISO M20 
- M12 => corresponds to PG13,5 

The cable entry M16 (1/2 NPT) is in discontinuation of marketing. So, it is possible to replace it by standard product ACW21M11 or M12 and add an adaptor 1/2 NPT /ISO M20 or PG13.5
 
Was this helpful?
What can we do to improve the information ?