Technical FAQs

Ask a Question

Would like to know the type of temp sensor; that is used at heatsink for ATV630 Drive temp protection.

The temperature sensor is a PTC type.
There is only one sensor installed on the ATV630 heatsink.
 
Was this helpful?
What can we do to improve the information ?