Technical FAQs

Ask a Question

What are the neccesary points to be checked for TM5 bus error?

For checking the TM5 bus error following things need to be checked:
* From where the supply is given to the TM5 bus expansion module? whether it follows all the wiring guidline 
  as per the harware guide. whether recommended supply is reaching or not in the TM5 bus?
* whether any overloading is happening on the TM5 bus?
* whether the configuration done on the somachine program and the configuration present physically is same or not?
Was this helpful?
What can we do to improve the information ?