Technical FAQs

Ask a Question

Can we use XVUZ12 with XVBC21B?

No we cannot use XVUZ12 with XVBC21B for XVUZ12, the dimension of the center hole is 23.5mm (+-0.15) and also there is another layer under this hole and its width is 18 mm (+-0.15).
Was this helpful?
What can we do to improve the information ?