Technical FAQs

Ask a Question

What is the filter processing error while using PID in Somachine Basic ?

Filter processing error (Error 0x8015) will happen if filter time < 10 x cycle time : for example filter time of 100 ms will not work with a cycle time of 20 ms. Here the cysle time is the scan time of the somachine basic application in which PID is used.
 
Was this helpful?
What can we do to improve the information ?