Technical FAQs

Ask a Question

How is imbalance factor calculated in EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420) for current imbalance protection

Imbalance factor for EOCR-i3DM (Z, S, 420) / iFDM (Z, S, 420) is calculated as follows:

Imbalance factor (%) = (Imax phase - Imin_phase) / Imax_phase x 100%
Was this helpful?
What can we do to improve the information ?