Technical FAQs

Ask a Question

What is the electrical characteristic of relay contact provided with PM1130H meter?

It is a Form A relay, 2 pins terminal type. 

300 V L-N max. at 2 A
24 V DC at 2A
Was this helpful?
What can we do to improve the information ?