Technical FAQs

Ask a Question

How to check the driver version of a particular driver in Vijeo Citect.

The driver version of a particular Citect driver (e.g. Modnet, OPC etc.) can be checked by checking the '.dll' file version which is installed along with the
driver. The installation path being as follows: 
C:\Program Files (x86)\Schneider Electric\Vijeo Citect 7.50\Bin

There are two ways to check the driver version.
- simply hover the mouse over the 'dll' file will pop out the details along with version (named as 'File version')
- Right Click the 'dll' file > Properties > Check the 'File version' under 'Details' Tab
Was this helpful?
What can we do to improve the information ?