Technical FAQs

Ask a Question

Calibration sensor is requested by the customer for Sensors' Portfolio.

If a calibration certificate is requested, this must be notified to the Orders dept when the order is placed. The ordered sensors are then tested again according to the specifications and delivered with a calibration certificate. This process may lead to additional costs and a slightly longer delivery time. Calibration certificates cannot be produced after the products are delivered.
Was this helpful?
What can we do to improve the information ?