Technical FAQs

Ask a Question

What is a PowerTag.

PowerTags comply to  IEC 61557-12 PMD/DD/K55/1 and are energy sensor modules for 1P, 1P+N, 3P and 3P+N networks.
They are mounted directly on equipment of the Acti 9 or Multi 9 range at intervals of 18 mm up to 63 A.
Was this helpful?
What can we do to improve the information ?