Technical FAQs

Ask a Question

What is the degree of protection of PowerTag.

The degree of protection of PowerTag is given below
  • Device only -> IP20
  • IK                -> 05
Was this helpful?
What can we do to improve the information ?