Technical FAQs

Ask a Question

What reports are available in the StruxureWare Building Operation Energy Reporting Pack.

The following reports are available in the StruxureWare Building Operation Energy Reporting Pack:

  • Energy Monitoring Calendar Consumption Report provides an interactive report that shows the energy usage on one or multiple selected days

  • Energy Monitoring Consumption Breakdown Report shows energy consumption broken down using sub-metering

  • Energy Monitoring Consumption Report shows the energy consumption against a specified target value

Was this helpful?
What can we do to improve the information ?