Technical FAQs

Ask a Question

What are the tasks which WebReports client performs in EcoStruxure Building Operation.

The WebReports client performs the following tasks:

  • Sends requests for reports

  • Administers the Reports Server

  • Provides the user interface for viewing, customizing, and managing reports

During the installation, the WebReports Installer installs the WebReports client on the computer where IIS is installed.

Was this helpful?
What can we do to improve the information ?